KAS Simulator Menus Description
File Menu
Command |
Description |
---|---|
Start |
Start the application with the Retain Variables. |
Cold Start |
Start the application with the initial settings. |
Stop |
Stop the application. |
Option |
Set parameters for the KAS Simulator application (see explanations below). |
Exit |
Leave KAS Simulator application. |
Option
Option |
Description |
---|---|
Autostart |
Autostart the application when KAS Simulator is launched. Autostart mode is recommended when a system is in production. |
-
-
Parameters are saved in the Options.bin file located under:
<user>\AppData\Local\Kollmorgen\KAS\Sinope Simulator\Resources\
Help Menu
Command |
Description |
---|---|
About |
Show version numbers and other Find the KAS-IDE Version about KAS Simulator |